ProcessorExpert and KDS project file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ProcessorExpert and KDS project file

1,435 Views
oaf
Contributor IV

Hi,

 

There is one issue regarding PEx and KDS which is quite annoying.

1. The PEx doesn't delete generated files from Beans removed from the project

2. The KDS project file compiles *.c

The net effect is that a PEx module which is removed, will be compiled with your project and may cause some

unwanted behaviour. Working one person may go right, if you are careful, but working in a multi-people project

will cause trouble.

I would like to have some kind of fix for this problem....

Labels (1)
0 Kudos
Reply
1 Reply

1,369 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ole,

can you please check if this properties setting can help you:

2015-05-27_12-13-35.png

if can't help, please specify more about your problem, I will check it further. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply