Processor Expert to KSDK-2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert to KSDK-2.0

2,437 Views
javierhernande1
Contributor IV

Hi!,

 

I have one FRDM-K64F-AGM01 and also one BRKT-STBC-AGM01.

I have tested some examples with mbed code and work. Both, the compiler online as exporting to KDS 3.0.2.

 

I have tried the FXO8700CQ integrated in the K64F with mbed code and works well. (i2c address 0x1d)  Test_FXOS8700CQ - a mercurial repository | mbed

 

I would try the Sensor ToolBox application but I think it is only available for Windows, I use Fedora 23 64bit.

 

Now, I would like to use the FRDM-K64F-AGM01 (both, K64F + STBC-AGM01) with Processor Expert and ISF 2.2 (Intelligent Sensig Framework).

 

I have installed KDS 3.0.2 (eclipse platform 4.4.2)

 

Processor Expert for KDS version -> 3.0.2b151214

Processor Expert KPSDK specific features -> 1.3.0.RT7_b1550-0615

Processor Expert Core -> 1.4.1.RT7_b1550-0615

Freescale Custom Actions Updater for Eclipse 3.7 and 4.2.x ( version 2.0.12)

 

Installed the Processor Expert PEupd file containing the ISF components  ISF R2P2 PEx.PEupd

 

Generated the SDK 2.0 to FRDM-K64F and added to Processor Expert Paths. (image 1)

 

152767_152767.pngpepaths.png

(image1)

 

 

I tried to create a new Processor Expert project but does not allow me to select the Kinetis SDK 2.0 in Rapid Application Development.  Only KSDK_1.3.0, KSDK manual selection or None.

 

Is it not possible to create a PE project with the SDK-2.0 or no other way for it?

 

 

Other question, I wanted to try this DataLogger created by David Munsinger but I can not see the images of the blog, tells me forbidden. Do you know if there is any way to see it? Or if in another place where it is displayed correctly?

 

Creating a Data Logger embedded application using the Intelligent Sensing Framework (ISF 2.1)

 

Best regards,

Javier

Labels (1)
2 Replies

1,449 Views
MarekTrmac
NXP Employee
NXP Employee

Hi Javier,

Processor Expert does not support KSDK2.0.

Erich Styger found workaround and made this working and he describe his solution on his blog, see for example: https://mcuoneclipse.com/2016/05/15/mother-of-components-processor-expert-with-nxp-kinetis-sdk-v2-0-...

KDS 3.2 contains New Project Wizard for SDK2.0 (creates projects without Processor Expert).

Regards

Marek

1,449 Views
javierhernande1
Contributor IV

Hi Marek,

Thanks for the reply.

I tried now Sensor Fusion Toolbox for Windows from the machine from a friend and it works.

Basically, what I need to do is expose the data from the sensors (Accelerometer, Gyro, Magnetometer :: FXOS8700CQ, FXAS21002C) via SPI to be retrieved by a microprocessor. FRDM-K64F as SPI slave and Microporcessor as SPI master.

I have KDS 3.2.0 installed in Fedora 23. ¿Can I use 'Sensor Fusion Library for Kinetis MCU 5.0' with KDS 3.2.0 and KSDK_2.0? Okay well?

Best regards.

0 Kudos
Reply