Processor Expert doesn't handle some alt function of a pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert doesn't handle some alt function of a pin

698件の閲覧回数
mastupristi
Senior Contributor I

Hallo,

 

I am working with Kinetis K64 lqfp 144, KDS 3.1 and Processor Expert 3.0.2.

Pin 47 is called PTE26/ENET_1588_CLKIN/UART4_CTS_b/RTC_CLKOUT/USB_CLKIN and can have some functions:

141342_141342.jpgpin_lqfp144.jpg

but processor expert doesn't manage ENET_1588_CLKIN function:

141343_141343.jpgPE.jpg

 

How can I set up the pin for ENET_1588_CLKIN function? Only by hand?

 

best regards

Max

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

580件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Max,

Yes , it only can configure the PTE26 to ENET_1588_CLKIN function by hand,

through the register of PORTx_PCRn -> MUX .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信