Processor Expert, cannot select ADC1_DP1 pin on K26

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert, cannot select ADC1_DP1 pin on K26

ソリューションへジャンプ
1,415件の閲覧回数
jesperpape
Contributor II

Hello,

 

I am setting up a project in Processor Expert (KDS 3.0.1) for a MK26FN2M0VMI18 MCU

 

It is not possible to select pin ADC1_DP1 as input for ADC1.

 

Anyone that can help fixing this?

 

BR

Jesper P. Larsen

ラベル(1)
0 件の賞賛
返信
1 解決策
1,329件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jesper,

I would recommend you to use Kinetis SDK 1.3 which is the latest release, in this version the  ADC1_DP1 pin is now routed to the ADC1 function:

pastedImage_0.png

you should be able to select it as input pin for channel 1:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,330件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jesper,

I would recommend you to use Kinetis SDK 1.3 which is the latest release, in this version the  ADC1_DP1 pin is now routed to the ADC1 function:

pastedImage_0.png

you should be able to select it as input pin for channel 1:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信