Processor Expert Library mode not working - platform_lib

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert Library mode not working - platform_lib

1,358 次查看
kylehamilton
Contributor II

I believe that the "platform_lib" library mode in the Processor Expert KSDK settings (see below) is not working.  I have created a project with and without this selected and I see no difference in the files that are copied or linked from the KSDK.  Even with this option selected, all of the fsl_*_driver files are still copied into my PE project.  Has anyone used this with success?

 

Note that I am using KDS 3.0 with KSDK 1.2.

 

61493_61493.pngpastedImage_0.png

 

Thanks,

Kyle

标签 (1)
0 项奖励
回复
1 回复

1,213 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kyle Hamilton:

I see the same behavior and I reported it already (ticket PEXMCU-3748).

I will let you know about any feedback I receive from the Processor Expert development team.

Regards!

Jorge Gonzalez

0 项奖励
回复