Problems with adc multiple channels using processor expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems with adc multiple channels using processor expert

跳至解决方案
2,127 次查看
maikonperin
Contributor I

I'm using kl46z and kinetis design studio to measure two adc channels but it's not working. I just added 2 channels on the processor expert.

I'm using the code below.

 

static uint8_t value[AD1_CHANNEL_COUNT];

(void)AD1_Measure(TRUE);

 

   AD1_GetValue8(&value[0]);

   AD1_GetValue8(&value[1]);

 

Can someone help me? Thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,870 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Perin,

When read the result , please write :

AD1_GetValue8((byte*)value);

For in the function of "byte AD2_GetValue8(byte *Values)" , it has include read the two channel result :

/* ===================================================================*/

byte AD2_GetValue8(byte *Values)

{

  if (OutFlg != 0x03U) {              /* Is output flag set? */

    return ERR_NOTAVAIL;              /* If no then error */

  }

  Values[0] = (byte)((byte)(AD2_OutV[0] >> 8U)); /* Save measured values to the output buffer */

  Values[1] = (byte)((byte)(AD2_OutV[1] >> 8U)); /* Save measured values to the output buffer */

  return ERR_OK;                      /* OK */

}

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,871 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Perin,

When read the result , please write :

AD1_GetValue8((byte*)value);

For in the function of "byte AD2_GetValue8(byte *Values)" , it has include read the two channel result :

/* ===================================================================*/

byte AD2_GetValue8(byte *Values)

{

  if (OutFlg != 0x03U) {              /* Is output flag set? */

    return ERR_NOTAVAIL;              /* If no then error */

  }

  Values[0] = (byte)((byte)(AD2_OutV[0] >> 8U)); /* Save measured values to the output buffer */

  Values[1] = (byte)((byte)(AD2_OutV[1] >> 8U)); /* Save measured values to the output buffer */

  return ERR_OK;                      /* OK */

}

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复