Problem using kinetis design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem using kinetis design studio

1,949件の閲覧回数
shravansrinivas
Contributor I

I have recently started working with keaz128 board. I needed a little help with programming with kinetis design studio. First up I want to make sure if I can use kinetis design studio for programming this board or should I be using s32 design studio?

While using Kinetis design studio I could not add a component to the project. Can anyone help me out with this?

( As the board I was using was not available I selected the processor during creation of new project)

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,809件の閲覧回数
shravansrinivas
Contributor I

Thank you for responding. I tried with the same processor as you have shown in the image. But nonetheless I'll try with s32.

Are there any tutorials for beginners?

0 件の賞賛
返信

1,809件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Shravan Srinivasa 

I want to make sure if I can use kinetis design studio for programming this board or should I be using s32 design studio?

KDS still support KEA family, but I would recommend to use s32 design studio, it is our lastest IDE for Automotive MCUs, which include KEA family.

When you mentioned that you couldn't add a component, you refer to a processor expert component? how are you creating your project? I could select and create a project selecting KEA128 processor, please check my image:

pastedImage_2.png

Then I could add componennts and compile and debug my project.

Regards

Jorge Alcala

0 件の賞賛
返信