Problem using J-LINK Segger debugger with KDS3.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem using J-LINK Segger debugger with KDS3.2.0

Jump to solution
2,091 Views
predragvidic
Contributor I

When try to debug my project, which builds without any problem, (Segger J-LINK) the KDS 3.2.0 replies: 'Launching my_project_name debug' has encountered a problem. Program file does not exist.

Also debugger continues to try to start and is continuously on 62%

I have followed the steps from the KDS user manual

0 Kudos
Reply
1 Solution
1,876 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Predrag.

This is a same question. please refer answer here

https://community.nxp.com/thread/463195


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,877 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Predrag.

This is a same question. please refer answer here

https://community.nxp.com/thread/463195


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply