Periodic Interrupt Source - which timer is best?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Periodic Interrupt Source - which timer is best?

1,927件の閲覧回数
Jiun_Yong
Contributor III

I am asking this out of general interest:

My application includes a 1 millisecond timer, which obviously generates an interrupt every millisecond.

When I create a Periodic Timer with Processor Expert, I am presented with a number of options for the Periodic Interrupt Source.:

1. One of the Timer/PWM Channels

2. One of the Periodic Interrupt Timers

3. Low Power Timer

But does anyone have some guidance on what is the "preferred" interrupt source?

What advantages does any option have over another?

 

(PS: for the record, I am working on KL26 and KL03 processors)

ラベル(1)
0 件の賞賛
返信
1 返信

1,620件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello STEVE,

If you only use the timer interrupt function , the three module all can  generates an interrupt every millisecond.

While the TPM mode can generate PWM signal ,Input capture mode and output compare ;

The PIT mode can generate DMA trigger pulses, only can be sued  to the  time cunt ;

The LPTMR can run at the five mode : Run, Wait , Stop, Low-Leakage, Debug .

So i think , if you only want generates an interrupt every millisecond , the PIT is enough, for

it can configuration  easily .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------