Parallel Build Prevents Pre/Post Build Commands

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallel Build Prevents Pre/Post Build Commands

2,439 次查看
leifzars
Contributor IV

Pre and Post build commands only run when Parallel build is disabled, when enabled they do not run.

Is this a bug?

 

Windows 7 KDS 3

标签 (1)
0 项奖励
回复
2 回复数

2,236 次查看
BlackNight
NXP Employee
NXP Employee

Hi Leif,

pre- and post-build steps work for me with parallel build enabled (using Win7 too). But there is a known issue in case you have custom per-file or per-folder options set, see Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse .

This is my setup:

pastedImage_1.png

Erich

0 项奖励
回复

2,236 次查看
leifzars
Contributor IV

... At lease it works for some. I guess I will create a test project.

And the link does not apply, i think.

It is very odd, I have two machines same setup same issue. and I am trying to compile the MQX psp and bsp for my board and the pre/post commands only run with parallel buildi off.

0 项奖励
回复