Parallel Build Prevents Pre/Post Build Commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parallel Build Prevents Pre/Post Build Commands

2,400件の閲覧回数
leifzars
Contributor IV

Pre and Post build commands only run when Parallel build is disabled, when enabled they do not run.

Is this a bug?

 

Windows 7 KDS 3

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,197件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Leif,

pre- and post-build steps work for me with parallel build enabled (using Win7 too). But there is a known issue in case you have custom per-file or per-folder options set, see Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse .

This is my setup:

pastedImage_1.png

Erich

0 件の賞賛
返信

2,197件の閲覧回数
leifzars
Contributor IV

... At lease it works for some. I guess I will create a test project.

And the link does not apply, i think.

It is very odd, I have two machines same setup same issue. and I am trying to compile the MQX psp and bsp for my board and the pre/post commands only run with parallel buildi off.

0 件の賞賛
返信