Open OCD for KEA-128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Open OCD for KEA-128

1,380件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

     Does KEA-128 support Open-OCD?

ラベル(1)
0 件の賞賛
返信
1 返信

1,187件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

according to KDS release note

KDS comes with OpenOCD (http://openocd.sourceforge.net/) with OpenSDA (http://www.freescale.com/opensda) debugging support. The following boards are supported with OpenOCD and CMSIS-DAP/mbed firmware on the board:

  • FRDM-KL02Z
  • FRDM-KL05Z
  • FRDM-KL25Z
  • FRDM-KL26Z
  • FRDM-KL46Z
  • FRDM-K22F
  • FRDM-K64F

All other boards not listed are considered as not supported (e.g. the FRDM-K20 is NOT supported with OpenOCD).

so KEA-128 doesn't support Open-OCD, Please use P&E OpenSDA or Jlink interface.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信