No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

跳至解决方案
3,309 次查看
leechakkhiam
Contributor II

Installing software encounter the following error. "No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534"

How to fix it?

Thank You.

标签 (1)
1 解答
2,852 次查看
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,853 次查看
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

0 项奖励
回复
2,852 次查看
leechakkhiam
Contributor II

Thank you. This solve the problems.

0 项奖励
回复
2,852 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Lee,

what's your system platform? version?

0 项奖励
回复
2,852 次查看
leechakkhiam
Contributor II

Hi ZhangJennie:

I am using 32bit xubuntu 14.04.

Thank you.

0 项奖励
回复
2,852 次查看
trytohelp
NXP Employee
NXP Employee

Hi Lee,

Sorry little late with my feedback.

See you've solved the problem.

On my side I'm able to create an build a project created with the project wizard for FRDM-K64F.

My configuration is:

  - Win 7 32 OS,

  - VirtualBox,

  - Ubuntu 14.04.1 (ubuntu-14.04.1-desktop-i386.iso)

  - KDS V1.1.0.

After to have installed the tool as root, the tool must be launch as root too:

  sudo /opt/Freescale/KDS_1.1.0/eclipse/kinetis-design-studio


This is working fine on my side.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------