NXP Application Engineer in Albuquerque New Mexico?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP Application Engineer in Albuquerque New Mexico?

2,307 次查看
ralphberger
Contributor I

I have TJA1100 phy design that the 1.8 power supply is measuring ~2.4 volts. The  design followed the applications guide and I would like get in contact with an FAE for this product line.

标签 (1)
0 项奖励
回复
3 回复数

1,934 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ralph,

Please contact your local agent of NXP .

BR

Alice

0 项奖励
回复

1,934 次查看
ralphberger
Contributor I

Hi Alice,

Thank you for replying back, could you please give the local NXP agents

contact information?

Regards,

Ralph G Berger

Integration Engineer

Innovasic, Inc.

5635 Jefferson St. NE, Suite A

Albuquerque, NM 87109

Office: +1 505.883.5263 x136 <505.883.5263%20x136>

Email: [email protected] <[email protected]>

www.innovasic.com <http://www.innovasic.com>

From: Alice_Yang

Sent: Tuesday, February 07, 2017 8:09 PM

To: Ralph Berger

Subject: Re: - Re: NXP Application Engineer in

Albuquerque New Mexico?

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: NXP Application Engineer in Albuquerque New Mexico?

reply from Alice_Yang

<https://community.nxp.com/people/Alice_Yang?et=watches.email.thread>

in *Kinetis

Design Studio* - View the full discussion

<https://community.nxp.com/message/874833?commentID=874833&et=watches.email.thread#comment-874833>

0 项奖励
回复

1,934 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ralph,

There is the distributors list :

http://www.nxp.com/buy/distributor-network:DISTRIBUTORS 

Hope it can helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复