Missing debug configuration DBG PEMicro Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing debug configuration DBG PEMicro Interface

1,371 Views
aidnani1
Contributor I

I am using a Mac. When I start KDS, and go to Run -> Debug Configurations… I do not see a configuration for 'DBG PEMicro …'. Any idea how I can get that for Mac?

Labels (1)
0 Kudos
Reply
1 Reply

1,178 Views
BlackNight
NXP Employee
NXP Employee

PEMicro does not have support for Mac OS X yet. But Segger J-Link is supported. If you are using a Freedom (FRDM) or Tower Board with OpenSDA, you can load the Segger firmware on it (OpenSDAv2​, Segger J-Link Firmware for OpenSDAv2, Freedom Board with Segger OpenSDA Debug Firmware), then it will be like a Segger J-Link and you can use it with Mac.

I hope this helps,

Erich

0 Kudos
Reply