Migrate from CodeWarrior 16.6 to KDS 2.0.0 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Migrate from CodeWarrior 16.6 to KDS 2.0.0 problem

ソリューションへジャンプ
1,558件の閲覧回数
EarlOrlando
Senior Contributor II

Hi,

 

I'm trying to migrate a project from CodeWarrior to KDS. I tried the steps listed in "C:\Freescale\KDS_2.0.0\doc\pdf\kds_porting_guide.pdf" but when I click in the "Convert CodeWarrior project file..." option, KDS does nothing. I tried reinstalling KDS 1.1.1 without success.

 

Does someone has experimented this problem? Is there another way to migrate the project without start from scratch?

 

FYI, my project has PEx components.

 

Best regards,

Earl.

ラベル(1)
タグ(5)
1 解決策
1,098件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Could it be that this project is not a gcc project? The converter will not convert non-gcc projects.

Erich

元の投稿で解決策を見る

2 返答(返信)
1,099件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Could it be that this project is not a gcc project? The converter will not convert non-gcc projects.

Erich

1,098件の閲覧回数
EarlOrlando
Senior Contributor II

Oh I see, it is not a gcc project.

Thanks Erich.

0 件の賞賛
返信