Method to download several program sections into different address in KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Method to download several program sections into different address in KDS?

2,253 Views
ConstYu
NXP Employee
NXP Employee

My customer mitsubishi is using KV5X and KDS, they want to know how to download several program sections into different address in KDS(no need to debug). Before they use CW, they use target task to download several program sections into different address like below,as it can assign the offset address. but i didn't find such function in KDS, is there any other method to achieve this target. thanks.

Untitled.png

0 Kudos
Reply
2 Replies

2,120 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Const,

There isn't the "Target Tasks" function in KDS.

While there is a method about protect some areas when flashing program,

please review this post to check whether it can work for you :

Updated P&E GDB Server for Eclipse: Connect/Attach and Advanced Flash Programming | MCU on Eclipse 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,121 Views
ConstYu
NXP Employee
NXP Employee

Hi Alice,

Thanks for your support, will make a try.

0 Kudos
Reply