Macro: Terminate, Clean, Build, Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Macro: Terminate, Clean, Build, Debug

2,082件の閲覧回数
ignisuti_
Contributor IV

Is there a way in KDS to setup a Hotkey/Macro to execute the following functions?

Terminate, Clean, Build, and then Debug

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,972件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Joe,

KDS3.0 doesn't have feature of define key bindings sequence.

it is more an eclipse feature.  here is some solution for eclipse:

FAQ How do I create my own key-binding configuration? - Eclipsepedia

Eclipse Commands Advanced - Tutorial

Define key bindings for Eclipse Commands - Tutorial

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,971件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Joe,

I suggest you go to IDE menu windows, preferences to view/modify the command hotkey.

see attached video.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信