Macro: Terminate, Clean, Build, Debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Macro: Terminate, Clean, Build, Debug

2,083 Views
ignisuti_
Contributor IV

Is there a way in KDS to setup a Hotkey/Macro to execute the following functions?

Terminate, Clean, Build, and then Debug

Labels (1)
0 Kudos
Reply
2 Replies

1,973 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Joe,

KDS3.0 doesn't have feature of define key bindings sequence.

it is more an eclipse feature.  here is some solution for eclipse:

FAQ How do I create my own key-binding configuration? - Eclipsepedia

Eclipse Commands Advanced - Tutorial

Define key bindings for Eclipse Commands - Tutorial

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,972 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Joe,

I suggest you go to IDE menu windows, preferences to view/modify the command hotkey.

see attached video.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply