MQX with PEG  tutorials

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX with PEG  tutorials

4,347件の閲覧回数
danieljackmorle
Contributor III

Looking in to a project that requires graphics and I am trying to use with the K70 board or K60 board.

Which one will have the most tutorials or examples.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,706件の閲覧回数
DaveTonyCook
Contributor IV

Hi Zhang,

Your link https://community.freescale.com/docs/DOC-101586 provides no information

0 件の賞賛
返信

3,706件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi dave,

this question was answered in 2014 and this article you mentioned is also old (written in 2014 too).  now it changes to version  5. I can't remember what exact it was two years ago.

If I am not wrong it should include a video at that time but now from my side the video can not be showed now.

as a suggestion you could leave your question to the article page, thus if  the author sees it he will know.

Jun

0 件の賞賛
返信

3,706件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Daniel,

please refer thread as below:

https://community.freescale.com/docs/DOC-101586

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

0 件の賞賛
返信

3,706件の閲覧回数
danieljackmorle
Contributor III

Do you have the files used in that demo on your web sight.

How do I get to the level in which I can do this using the kits.

Date: Fri, 10 Oct 2014 01:19:53 -0700

From: [email protected]

To: [email protected]

Subject: Re: - MQX with PEG tutorials

MQX with PEG tutorials

reply from ZhangJennie in Kinetis Design Studio - View the full discussion

Hello Daniel,

please refer thread as below:

https://community.freescale.com/docs/DOC-101586

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Kinetis Design Studio by email or at Freescale Community

Following MQX with PEG tutorials in these streams:

Inbox

0 件の賞賛
返信

3,706件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Daniel.

I suggest you check TWR-K70F120M + TWR-LCD-RGB  samples here:

PEG Software Product Line (GUI)|Freescale

PEG Medical Kiosk: Software offered 'As is', support provided on Freescale Communities only – Example PEG Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2220 Format: exe Rev #: 1.0 Modified: 8/29/2012
FREESCALE
Download
Favorite
PEG MQX HVAC: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2868 Format: exe Rev #: 1.0 Modified: 8/29/2012
FREESCALE
Download
Favorite
PEG MQX Web Security: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2732 Format: exe Rev #: 1.0 Modified: 8/29/2012

Hope this helps!

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

0 件の賞賛
返信