MQX Menu Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX Menu Missing

1,981件の閲覧回数
sueneal
Contributor I

While trying to debug my program I noticed the MQX menu has disappeared.

MQX RTOS plug ins are installed.

Have tried uninstalling and re-installing the plug in to no avail.

124740_124740.pngpastedImage_0.png

Any idea how I can get it back without reinstalling kds from scratch?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,861件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Sue,

Please make sure you have the Debug perspective open, the MQX menu only shows up on this perspective:

pastedImage_0.png

On the C/C++ Perspective the MQX menu is not visible:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,861件の閲覧回数
takmingmarcopan
Contributor II

G'day! I installed the files correctly on my old laptop and it worked marvelously!
However when i installed KDS 3.2 with MQX 4.2 today, i could not find the dropdown menu even in debug perspective. Got any ideas? 

Thank you!

0 件の賞賛
返信

1,861件の閲覧回数
sueneal
Contributor I

Sorted it.

0 件の賞賛
返信