Linux Setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Setup

1,242 Views
tonymakkiel
Contributor III


Hi,

     Is there a document on how to setup KDS on linux? I have KDS 3.2.0 installed. But cant get it to talk to the board(TWR-KL43Z48M) I have. I have tried copying the "hello_world.bin" to sda memory. I do not get the ttyACM0 interface anymore and not sure where the look for the output. I am guessing, I should modify one of the Debugconfiguration. But not sure how.

 

Can somebody please help?

 

Many Thanks,

Tony

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,043 Views
tonymakkiel
Contributor III

For anyboady who is stuck, with the same problem, managed to get the KDS debugger running using the following 2 links

Download the CMSIS-DAP Debug Application for OpenSDAv1 bin from

OpenSDA Serial and Debug Adapter|NXP 

Follow the instructions for KDS  in

OpenSDAv2

Oddly, I cant just run the application. But has to use the debug option within KDS.

0 Kudos
Reply