LWIP 2.0.0 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP 2.0.0 problem

2,554 Views
a8Chcx
Contributor IV

Hi,

I am using KDS3.2.0 with LWIP 2.0.0 on K66. I am using sample httpd web server and found the following problem:

Sometime, I got "LWIP_ASSERT("tcp_input: pcb->next != pcb (before cache)", pcb->next != pcb);" and stop working.

Can anybody tell me how to fix this issue?

Thanks,

Christie

0 Kudos
Reply
3 Replies

2,383 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Christie:

Currently LwIP version in latest SDK is 2.1.2.  If possible, I would suggest you update to latest version of SDK. 2.6.0.

You can download SDK from below link.

Welcome | MCUXpresso SDK Builder 

For your issue, it seems your application code is violating LwIP requirement.

Please read the following link for more details

lwIP: Common pitfalls 

Regards

Daniel

0 Kudos
Reply

2,383 Views
a8Chcx
Contributor IV

Hi Daniel,

Thank you for your information.

I am using KDS3.2.0 with KSDK2.2. Is there any easy way to upgrade LWIP stack without affecting others in my project? Otherwise, I have to use the new IDE and re-do all for my project...There are lots of work related to this...

Could you tell me if I can only update the files related LWIP stack?

Thanks,

Christie

0 Kudos
Reply

2,383 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, it is possible to update LwIP.

Please look at below link for the list of changes between different LwIP versions.

UPGRADING - lwip.git - lwIP - A Lightweight TCPIP stack 

Regards

Daniel

0 Kudos
Reply