LCDC component problem with Blink Rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCDC component problem with Blink Rate

2,177件の閲覧回数
720adams
Contributor I
If the K70 was supported in mcuxpresso, this issue might be a mute point.  However, because NXP has not added the K70 into mcuxpresso as one of the supported processors and their only suggestion is to use KDS, well here is a KDS bug that needs fixing.  Hopefully, they won't just ignore this.
The another bug is in the LCDC_LDD component for the TWR_K70 that comes with KDS.  The HW cursor initialization tab has a box to allow blinking to be turned on and the "Blinking rate" to be set from 1 to 255.  Turning blinking on works when the code is generated, but the blinking rate has no effect.  The component uses the default value of 0xFF that is set at system reset.  Changing the value manually indeed changes the Blinking rate so it is not a hardware issue but a component generation  issue.
Thoughts?
0 件の賞賛
返信
1 返信

2,106件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Michael,

 

Thank you for the information. I am going to send this feedback with design team.

 

Thanks for bringing this to our attention.

 

Best regards,

Felipe

0 件の賞賛
返信