Kinetis Windows 10 Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Windows 10 Support

ソリューションへジャンプ
1,916件の閲覧回数
neilporven
Senior Contributor I

Hi everyone,

 

Does Kinetis now support Windows 10?

It seems my PC is forcing me to go from window 7 to 10, which I have no problem with since is free, but

I work with Kinetis and the last time I checked, Kinetis didn't support Windows 10.

 

On the NXP website, there seems to be a little confusion as to weather it does or doesn't????  

 

This illustration shows it doesn't:

 

 

and much further down, I see the following:

 

Features

 

  • Eclipse Luna 4.4
  • Host operating systems:
    • Windows® 7/8/10 (32 and 64-bit)
    • Linux® 64-bit (Ubuntu 10.04 (deb), RedHat/Centos 7 (rpm))
    • Mac OS X (10.10 and 10.11) with SEGGER J-Link support

 

 

Can someone from NXP shed some light on this matter and possibly alert the Website personnel....

 

Thanks,

Neil Porven

ラベル(1)
0 件の賞賛
返信
1 解決策
1,591件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Neil

KDS 3.2.0 works well on a Windows 10 machine. It can be downloaded from:

Kinetis Design Studio Integrated Development Enviro|NXP


Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,592件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Neil

KDS 3.2.0 works well on a Windows 10 machine. It can be downloaded from:

Kinetis Design Studio Integrated Development Enviro|NXP


Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------