Kinetis KwikStik

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KwikStik

1,116 Views
lijofrancis
Contributor III

Dear sir,

              We buy board Kinetis KwikStik(k40) Board.I found problem is that the connector pin out PTE7 (B21) in user"s manual not the same pin.It is actually PTE11.please check any further change

Labels (1)
0 Kudos
Reply
1 Reply

977 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Lijo Francis,

I attached you the explanation for your answer.

http://cache.freescale.com/files/32bit/doc/ref_manual/KWIKSTIKK40UM.pdf?fpsp=1pte7__.png

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P144M100SF2RM.pdf

PTE7_.png

UART5 is a signification (name) on the board, it is not in connection with the chip. The signification (name) on the chip is UART3, so UART3RTS and is pin PTE7.

On port PTE11 is UART5RTS.

Best Regards,

Iva

0 Kudos
Reply