Kinetis Design Studio Update 3.1.0 failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio Update 3.1.0 failed

1,663件の閲覧回数
klausforstner
Contributor I

I tried to update the KDS 3.0.0 as described in the NXP Newsletter without success.

 

The downloaded file is:

139327_139327.pngpastedImage_1.png

Extracted locally and choosen by local:

139334_139334.pngpastedImage_2.png

 

And the result is always:

139326_139326.pngpastedImage_0.png

 

 

Did anyone know the reason?

I already re-installed the KDS 3.0.0 without any change

 

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

1,158件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

You can find installation instructions release notes included in the ZIP file you downloaded. It is recommended to use "Check for updates" instead of "Install new software". Installation instructions contains step-by-step process:

1. Run KDS 3.0.0

2. Select Window > Preferences

3. Select Install/Update > Available Software Sites

4. Add a new install site using the Add... button

5. Type name of the install site into the Name field (e.g. KDS 3.1.0).

6. Click on the Archive... button and find the KDS_3.1.0.zip.

7. Confirm site addition by clicking on OK button.

8. Close Preferences windows by clicking on OK button.

9. Select Help > Check for Updates

10. Continue with the wizard. Accept the license agreement during the installation process.

11. Restart KDS.


0 件の賞賛
返信