Kinetis Design Studio IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio IDE

3,065件の閲覧回数
doug_foss
Contributor I

I just downloaded Kinetis Design Studio IDE. I want to use the KL27Z parts and the FRDM-KL27Z board, but they are not listed in processor/board list. Is there a patch/update for this family of parts? If not, what is the closest other family to work with from a hardware/code standpoint?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,759件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Additional devices are supported with the Kinetis SDK.

See "For full/additional device support"  in New Kinetis Design Studio V3.0.0 available

I hope this helps,

Erich

0 件の賞賛
返信

2,759件の閲覧回数
doug_foss
Contributor I

Erich,

Ok, thanks for that link. I am not able to do the Help>Install New Software successfully however. I get the messages in the attached screenshot. Is there a step that I need to perform before this, or maybe I need to reinstall the KDS?

Thanks,

Doug

0 件の賞賛
返信

2,759件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have seen such things with either slow or unreliable internet connections.

Maybe you can disable 'contact all update sites' (see Workaround for “Installing Software has encountered a problem” in Eclipse | MCU on Eclipse ) if this has a positive effect?

Erich

0 件の賞賛
返信