Kinetis Design Studio IDE for Linux fails installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio IDE for Linux fails installation

ソリューションへジャンプ
3,164件の閲覧回数
lullytroconis
Contributor II

Hi Community.

Someone install KDS IDE on Linux?

I downloaded the Installer Kinetis Design Studio installer for Linux 64-bit DEB 3.0.0 I have Debian 7, but I have troubles with the installation:

# dpkg -i /home/lully/Descargas/Kinetis\ Desing\ Studio\ installer\ for\ Linux\ 64-bit\ DEB\ 3.0.0.deb

(Leyendo la base de datos ... 158354 ficheros o directorios instalados actualmente.)

Preparando para desempaquetar .../Kinetis Desing Studio installer for Linux 64-bit DEB 3.0.0.deb ...

Desempaquetando kinetis-design-studio (3.0.0) ...

dpkg-deb (subproceso): no se puede copiar el miembro del archivo de '/home/lully/Descargas/Kinetis Desing Studio installer for Linux 64-bit DEB 3.0.0.deb' a la tubería de descompresión: fin de fichero o de flujo inesperado

dpkg-deb: error: el subproceso copiado devolvió el código de salida de error 2

dpkg: error al procesar el archivo /home/lully/Descargas/Kinetis Desing Studio installer for Linux 64-bit DEB 3.0.0.deb (--install):

no se pudieron copiar los datos extraídos de 'opt/Freescale/KDS_3.0.0/doc/info/make.info-1' a '/opt/Freescale/KDS_3.0.0/doc/info/make.info-1.dpkg-new': fin de fichero o de flujo inesperado

Se encontraron errores al procesar:

/home/lully/Descargas/Kinetis Desing Studio installer for Linux 64-bit DEB 3.0.0.deb

I followed the installation steps.

I should be grateful if you could help me.

Regards.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,777件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Lully,

you can find MD5 signature on the NXP web site, see attached picture. It can be used to verify, if the file is downloaded correctly.Capture.PNG

元の投稿で解決策を見る

4 返答(返信)
2,777件の閲覧回数
gabrielrosapaz
Contributor I

Hi Lully.

I installed on my laptop with Ubuntu 14.04 (64-bit) and I had no problems. In fact I had a problem yes, but not in the installation, but when performing the build, I had to install packages and GCC 32bit and some libraries (libs) for 32bit.

Here are some tips that can help you:

1) Does the file was not corrupted in the download?

2) Try copying the file to /opt, access the directory and there to make the installation procedure.

2,777件の閲覧回数
lullytroconis
Contributor II

Hi Gabriel, I dowloaded 3 times the installer, but the error continues, I tried of the second option but nothing yet.

Thak you so much for the answer.

0 件の賞賛
返信
2,778件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Lully,

you can find MD5 signature on the NXP web site, see attached picture. It can be used to verify, if the file is downloaded correctly.Capture.PNG

2,777件の閲覧回数
lullytroconis
Contributor II

Hi Marek and Gabriel, I could install it! :smileyhappy: the download was corrupt. Thank you so much for help me.

0 件の賞賛
返信