Kinetis AsyncroSerial Error "IgnoreEOF"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis AsyncroSerial Error "IgnoreEOF"

2,096 Views
jfortuny
Contributor II

Hello

 

I am migrating from Colfire V1 to Kinetis MK10 using Kinetis Studio 3.0.

 

In the AsyncroSerial component I don't need buffers because I use my own buffers and in ColdFire works perfect. Always that I try to set the Input Buffer Size and the Output Buffer Size and generate code I get this error:

 

"Generator: FAILURE: at line 1822: Unknown macro: "IgnoreEOF" (file: Drivers\Kinetis\AsynchroSerial.drv)"

 

If I set the size other than 0 this error disappear.

 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

1,958 Views
TICS_Fiona
NXP Employee
NXP Employee

Sorry that I cannot reproduce this problem with KDS3.0.

I attached the project that I’m using.  Is the same problem appearing on your side?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,958 Views
jfortuny
Contributor II

Hello

Many thanks.

I attach my project.

Best regards

Juan David Fortuny

De: TICS_Fiona

Enviado el: jueves, 18 de junio de 2015 3:04

Para: Juan Fortuny

Asunto: Re: - Kinetis AsyncroSerial Error "IgnoreEOF"

Xin Kuang <http://jiveon.jivesoftware.com/mpss/c/nAA/PDcDAA/t.1nz/0srzjEDQSD2EIYDulMDWpA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTAjVmQMvAqFYCzr7mrjuZFDrhrjaOucPJVpJ-2FuAx0txG6ZfShQh8kM0bdX-2F-2BNcXcQ-3D> in Kinetis Design Studio - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/nAA/PDcDAA/t.1nz/0srzjEDQSD2EIYDulMDWpA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSAWJNSIwm-2FlO8kfOTaTQo8fAGi-2BQAb6VLkAX2xRDM4KOb5aep3fYcOBcUTDKtz0i4-3D>

0 Kudos
Reply

1,958 Views
jfortuny
Contributor II

Hello

Many thanks

Here is the project.

Best reagrds

Juan David Fortuny

De: TICS_Fiona

Enviado el: jueves, 18 de junio de 2015 3:04

Para: Juan Fortuny

Asunto: Re: - Kinetis AsyncroSerial Error "IgnoreEOF"

Xin Kuang <http://jiveon.jivesoftware.com/mpss/c/nAA/PDcDAA/t.1nz/0srzjEDQSD2EIYDulMDWpA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTAjVmQMvAqFYCzr7mrjuZFDrhrjaOucPJVpJ-2FuAx0txG6ZfShQh8kM0bdX-2F-2BNcXcQ-3D> in Kinetis Design Studio - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/nAA/PDcDAA/t.1nz/0srzjEDQSD2EIYDulMDWpA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSAWJNSIwm-2FlO8kfOTaTQo8fAGi-2BQAb6VLkAX2xRDM4KOb5aep3fYcOBcUTDKtz0i4-3D>

0 Kudos
Reply