Kinetics design studio repository problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetics design studio repository problem

10,171件の閲覧回数
blownelco
Contributor I

Ik krijg volgende foutmelding bij het zoeken naar updates en het installeren van new software in Kinetics Design Studio V3.2.0

 

No repository found at http://gnuarmeclipse.sourceforge.net/updates.

 

Iemand een idee wat er mis is?

ラベル(1)
15 返答(返信)

9,539件の閲覧回数
ice_hevean
Contributor I

Hi all,

I have tried to put the zip file into the Kinetis and get the pyocd debugger but seems not working. Any ideas?


caanotperform.png
Thank you!

Best regards,

Frances

0 件の賞賛
返信

9,539件の閲覧回数
sys
Contributor III

Hello,

I have the same problem, specifically for the repo "http://gnuarmeclipse.sourceforge.net/updates". I get the error: 

"No repository found at http://gnuarmeclipse.sourceforge.net/updates."

It's a bit that i have this problem, I search around but it seems the URL is ok, is there some other problems?

Thanks,

Sandro

0 件の賞賛
返信

9,539件の閲覧回数
vlorenzop
Contributor II

Sandro, I'm experiencing this same issue too. I found some references to strong encryption changes applied by sourceforge as root cause for some similar issues and applied the patches as suggested by Oracle. The original error I was experiencing is the one described here: GNU ARM Eclipse plug-ins: Received fatal alert: handshake_failure.

Have you succeeded on solving this issue?

9,539件の閲覧回数
sys
Contributor III

Hello Victor,

thanks for writing and helping. I just tried your suggestion, but it doesnt work for me.

I replaced the jars in every version of JRE and JDK I have, but the result is the same.

I also get the handsdhake_failure stuff, but the JCE files doesnt solve the problem.

It is frustating that anyone in NXP dont know the solution...it is a bit that I posted the question...

I didnt understand: for you this solved the issue? Maybe the jars have to be placed in some other places than the standard java path? Maybe there are new version of the jars?

Thanks again for the time you took for me!

Sandro

0 件の賞賛
返信

9,539件の閲覧回数
vlorenzop
Contributor II

Sandro, I'm sorried, but I've not been able to solve it yet. I gave some more info to Alice in my post a little bit up in this thread here: (https://community.nxp.com/message/874633?commentID=874633#comment-874633).

In my case, for solving the security exception (ProvisionException) in Java, I had to copy the jars in the JRE that comes with KDS, in my installation there was a copy in folder C:\Freescale\KDS_v3\eclipse\features\com.somniumtech.jre.win32.win32.x86_1.7.0.76\jre\lib\security. After doing that my error changed from java security exception (handshake_failure) to repository not found.

I've posted a question in the support forum for the GNU ARM Eclipse plug-ins, here: GNU ARM Eclipse Plug-ins update site not working? | element14 | GNU ARM Eclipse .

I'll let you know if anyone replies with a working solution.

Regards, Victor

9,541件の閲覧回数
BlackNight
NXP Employee
NXP Employee

What worked for me is (as a workaround):

1. Download the zip file from GNU ARM Eclipse Plug-ins Releases 

2. In KDS/Eclipse, use menu Help > Install New Software and then point to the zip file (or use drag&drop):
pastedImage_2.png

9,541件の閲覧回数
vlorenzop
Contributor II

Thanks a lot Erich,

Have you tested the J-Link debugging plug-in that comes with the latest release?

One more question, do you use to make regular updates of the J-Link support that comes with the KDS? Any recommendations/thoughts about it?

0 件の賞賛
返信

9,541件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Victor,

I have not formally tested it, but I'm using with KDS V3.2.0

    GNU ARM C/C++ J-Link Debugging    4.1.2.201701141320

    Segger J-Link Software V6.12i

in my daily work and that works well for me.

Erich

0 件の賞賛
返信

9,541件の閲覧回数
vlorenzop
Contributor II

Thanks again!

Regards, Victor

0 件の賞賛
返信

9,539件の閲覧回数
sys
Contributor III

Thanks Erich,

so there is an open issue about this.

Thank you for the temporary workaround! We wait for the solution with no hurry now :smileyhappy:

Regard,

Sandro

0 件の賞賛
返信

9,539件の閲覧回数
sys
Contributor III

Thanks Lorenzo, now the first issue is gone!

...a very easy to find java-path :smileywink: I supposed that could be another ( ! ) RE installation but I couldnt find it.

Now I am in your same condition, I hope someone will help us...

Keep me informed, thank you again!

Regards

Sandro

0 件の賞賛
返信

9,539件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kurt,

Sorry i can't understand your question , could you please describe it in English, thank !

BR

Alice

0 件の賞賛
返信

9,539件の閲覧回数
blownelco
Contributor I

Hello,

I'm getting the follwing error while updating/installing new software in  Kinetics Design studio V3.2.0

Some sites could not be found.  See the error log for more detail.
No repository found at http://download.eclipse.org/tools/emf/updates/.
No repository found at http://www.eclipse.org/modeling/emft/?project=search#search.
No repository found at http://gnuarmeclipse.github.io.

Anyone an idea what is wrong with Studio, i just starting with it and need to  install pyocd.

0 件の賞賛
返信

9,539件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kurt,

The second site you mentioned can open on  KDS , the steps as below:

click Help ->Install New Software...

pastedImage_1.png

Input the site into Work with-> click Enter-> wait a while , it will show :

pastedImage_2.png

Hope it heps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

9,539件の閲覧回数
vlorenzop
Contributor II

Ok Alice, it worked for you, but not for some of us.

Did your software support/maintennance team applied any change in your Java or KDS installation lately? Maybe one of your collegues knows a working solution for this issue?

In my case, when trying to access manually the update site (direct download of the content.xml file), the response from sourceforge is

The "/Eclipse/updates-tes..tes-test/content.xml" file could not be found or is not available.  Please select another file.

It makes me think that maybe the update site has changed. Do you know of any alternative update site for upgrading the GNU ARM pluggins in KDS?

Regards Victor

0 件の賞賛
返信