KDS3.2 Building Qestion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS3.2 Building Qestion

2,690 Views
tfl166
Contributor I

Hi:

      My Project ,use kds3.2 to building project,but behave this question:

       Build project error: 

                                        error: "include "SKEAZ1284.h" ,no such file or directory

                                         this file and directory in Project /properties/Tool Setting/Corss ARM C Compiler/include already                                                add it?

             Why?

              Please to recall it !thks!

0 Kudos
Reply
5 Replies

2,462 Views
tfl166
Contributor I

Hi!

    I use a sample good project! To copy old behave" question file" to sample project ,

    Renew this file and directory in Project /properties/Tool Setting/Corss ARM C Compiler/include.

    reBuilding is OK!

    No change sub file!

    Why? 

    thks!

                                                                                          Tailor

0 Kudos
Reply

2,462 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

check that Include path in your project are properly configured. Use project properties to review. See attached screenshot.

Capture.PNG

Hope this helps.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

2,462 Views
jerrytomlee
Contributor II

I have encounter the simlar problems using S32DS., after the files into a new project, problems sovled. wonder why?

0 Kudos
Reply

2,462 Views
tfl166
Contributor I

Marek:

          Please give me Email! I mail my project file to you!

         thks

0 Kudos
Reply

2,462 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Could you please share your project ?

BR

Alice

0 Kudos
Reply