KDS v3.0.0 Environment Setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS v3.0.0 Environment Setup

2,074 Views
bradleyhiggin
Contributor I

To whom it may concern:

 

I downloaded and installed the following:

"Kinetis Design Studio installer for Microsoft Windows 3.0.0.exe"

"PEx_for_Kinetis_3.0.1.zip"

 

However, I have no idea what to do with:

"KDS v3.0.0 Source Files Package.zip"

 

Thanks in advance,

 

Brad

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,562 Views
BlackNight
NXP Employee
NXP Employee

Hi Brad,

The open source policy requires that any changes of the base sources used shall be published. So if you want to rebuild the open source parts of KDS on your own, then you need these files. Otherwise, if you don't plan to build your own toolchain, it is not needed.

Erich

0 Kudos
Reply

1,562 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bradley,

About use KDS on Windows , do not need care about this "KDS v3.0.0 Source Files Package.zip" .

And after you install KDS 3.0, i recommend you install KSDK1.3 , for some chips  driver are supported on the KDSK1.3,

you can download it here :

Software Development Kit for Kinetis MCUs|Freescale

and about how to install it in KDS,  please refer to the DOC of "KDS_Users_Guide.pdf"(under the installation directory of KDS : Freescale\KDS_3.0.0\doc)

pastedImage_0.png

Hope it helps

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


Have a great day

Alice

0 Kudos
Reply