KDS uC/OS-III error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS uC/OS-III error

885件の閲覧回数
xtrm
Contributor I

Hello,

I'm trying to create new KDS project with OS uc/OS-III but I have some problems with it. I use KDS 3.1.0 and KDSK 1.3.0. When I add uc/OS-III to the project I get two errors:

 

Description    Resource    Path    Location    Type

Error in the inherited component settings (uCOSIII)    test        osa1/uCOSIII    Processor Expert Problem

141804_141804.jpg1.jpg

 

Description    Resource    Path    Location    Type

ERROR: Cpu component name is in collision with uCOSIII source file (uCOSIII contains cpu.h file). Please rename the Cpu component.    test        ucosIII    Processor Expert Problem

141805_141805.jpg2.jpg

As I indicated on screenshot Component name can't be changed. Could anybody help me? Thank you.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)