KDS target task

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS target task

Jump to solution
2,254 Views
alubeiro
Contributor IV

Hi all,

 

I wonder if it is any tool or option in KDS similar to target task in CW.

I am developing a bootloader and want to load the app without deleting the boot.

 

How could i delete a certain bunch of addresses leaving the rest of them as they were.

 

167044_167044.pngpastedImage_1.png

167048_167048.pngpastedImage_2.png

 

Any help will be appreciated.

 

Thanks and best regards

Labels (1)
0 Kudos
Reply
1 Solution
2,147 Views
DavidS
NXP Employee
NXP Employee
0 Kudos
Reply
3 Replies
2,147 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Alberto,

Yes, refer to the tutorial David suggest above , configure the Memory Preservation

to preserved range of memory maintained through erase/program .

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,147 Views
alubeiro
Contributor IV

Hi David, Alice

Thanks for your quick response.

Best regards

0 Kudos
Reply
2,148 Views
DavidS
NXP Employee
NXP Employee

Hi Alberto,

Please review this post to see if it works for you.

https://mcuoneclipse.com/2015/04/16/updated-pe-gdb-server-for-eclipse-connectattach-and-advanced-fla... 

Regards,

David 

0 Kudos
Reply