KDS recipe for target ... failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS recipe for target ... failed

1,958件の閲覧回数
chadwilliams
Contributor III

Hello all,

 

I have come across this problem where the build is failing and I am seeing numerous errors in the build console such as this :

 

c:/freescale/kds_v3/eclipse/../bin/sh: syntax error: unterminated quoted string
rtos/freertos_8.2.3/Source/subdir.mk:33: recipe for target 'rtos/freertos_8.2.3/Source/tasks.o' failed

 

It looks as though KDS is not recreating the .mk files correctly and is causing the syntax error

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,003件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Chad,

Is this problem happening with that specific project? Was this project originally created in KDS 3.2? Could you also tell us which MCU are you using?

I once had a similar problem with a project and it was caused because the include paths on the project settings did not had quotation marks, maybe this is the case?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信