KDS not allowing addition of components

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KDS not allowing addition of components

跳至解决方案
2,091 次查看
noobletmoar
Contributor I

Hi,

When I try to add components from components library, the "Add to project" option is greyed out. It says "No project focused, all components displayed".

Here's a screenshot of the KDS. Please advise.

 

166843_166843.PNGsome phail.PNG

标签 (1)
0 项奖励
回复
1 解答
1,582 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

from your screenshot. the "Test" project is not a processor expert project.

please create a processor expert based project(see below screenshot), then import pe component. See how it works.

Whether the project supporting SDK is ok. the important is the project itself must support pe.

pastedImage_1.png

For a pe project, under the project folder, there must be a *.pe file. please check it on your side.

pastedImage_2.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,583 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

from your screenshot. the "Test" project is not a processor expert project.

please create a processor expert based project(see below screenshot), then import pe component. See how it works.

Whether the project supporting SDK is ok. the important is the project itself must support pe.

pastedImage_1.png

For a pe project, under the project folder, there must be a *.pe file. please check it on your side.

pastedImage_2.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,582 次查看
noobletmoar
Contributor I

Thanks for the response, it worked. However, is there no Processor Expert support for KSDK2.0?

0 项奖励
回复
1,582 次查看
BlackNight
NXP Employee
NXP Employee

No, there is no Processor Expert support for Kinetis SDK 2.0 (see https://mcuoneclipse.com/2016/01/29/first-nxp-kinetis-sdk-release-sdk-v2-0-with-on-demand-package-bu... ).

There is only the way that you can carry over the generated code, see https://mcuoneclipse.com/2016/05/15/mother-of-components-processor-expert-with-nxp-kinetis-sdk-v2-0-... .

I hope this helps,

Erich

0 项奖励
回复