Hi,
after downloading "Design Studio installer for Linux 64-bit RPM 3.0.0.rpm" I wanted to install it an on a CentOS Linux 7 machine, I'm facing the following problem:
[dev@localhost vm_share]$ sudo rpm -Uvh Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ RPM\ 3.0.0.rpm Preparing... ################################# [100%] Updating / installing... 1:kinetis-design-studio-3.0.0-1 ################################# [100%] error: unpacking of archive failed on file /opt/Freescale/KDS_3.0.0/eclipse/features/com.somniumtech.jre.linux.gtk.x86_64_1.7.0.76/jre/lib/jfxrt.jar;55ed5cb9: cpio: read failed - No such file or directory error: kinetis-design-studio-3.0.0-1.x86_64: install failed
any hint ?
已解决! 转到解答。


Hi Peter,
Currently I have only CentOS 6.6 where I checked that the installation works well so until I'll get CentOS 7 installed:
- Could you please check md5 checksum of your download? It should be 1a7709693e49c16fa7a7cc6a4627ece8.
- I noticed that you used rpm -Uvh (upgrade) command - does it mean that you already have some KDS installed?
Regards,
Lukas


Hi Peter,
Currently I have only CentOS 6.6 where I checked that the installation works well so until I'll get CentOS 7 installed:
- Could you please check md5 checksum of your download? It should be 1a7709693e49c16fa7a7cc6a4627ece8.
- I noticed that you used rpm -Uvh (upgrade) command - does it mean that you already have some KDS installed?
Regards,
Lukas
I was inspired from this document:
http://cache.freescale.com/files/microcontrollers/doc/user_guide/KDSUG.pdf?fsrch=1 , page 6
To install the Kinetis Design Studio software development tools on an Linux Standard Base (LSB)-compliant system, use the .rpm package file.
$ sudo rpm -Uvh kinetis-design-studio-3.0.0-1.x86_64.rpm
Preparing ... ########################################### [100%]
1: Kinetis Design Studio ########################################### [100%]
This will install the Kinetis Design Studio software development tools to the default location (/opt/Freescale/KDS_3.0.0).
if this is wrong, you should probably update the guide....
I was in a hurry to get the linux environment up and running so ditched my CentOS 7 efforts in favour a Ubuntu 14.04.
regarding the rpm file: our firewall proxy decided to cancel the download at some point. your assumptions are correct: the rpm file was broken.
thanks for the attention!


Hello Peter,
What about the extension of the KDS file , please change the extension to .deb , then have a try .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
eerrmm....
mind you: CentOS is rpm based... why would I change the file extension to .deb ??
ok.. you could use the Alien package to convert a package form rpm to deb... Alien - Debian Wiki
but hey... WHY ?
No Peter, you are correct on this one. the RPM package is the proper one for CentOS.
If a fresh download did not work, then there is another problem. Regarding Alien, it would make more sense if "plan-B" were to convert the prepackaged .deb into an .rpm file to use. I do not recommend this however.
sudo rpm -ivh Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ RPM\ 3.0.0.rpm
-i for install...