KDS debugging doesn't terminate existing connection automatically when new session starts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KDS debugging doesn't terminate existing connection automatically when new session starts

跳至解决方案
981 次查看
petershih
Contributor III

I have a question regarding KDS IDE. We have been using CW 10.6 to develop many application already. When debugging at CW, if a new source code is compiled and ready to be downloaded to the target, the CW will shows a warning message and able to automatically terminate the existing connection and start the new one. When I switch to KDS for debugging, it always give me "No Device Available" error. I have to "Abort" twice, switch to "Debug" perspective to terminate the existing connection.

83437_83437.jpgpastedImage_0.jpg

Do I have any way to set it automatically terminate the existing connection and start the new connection right away? Thanks your help!

 

Peter Shih

标签 (1)
0 项奖励
回复
1 解答
852 次查看
BlackNight
NXP Employee
NXP Employee

Hi Peter,

The bad news first: the P&E launch configuration in Eclipse does not support that functionality.

In CodeWarrior, this is handled by the custom debugger engine, and CodeWarrior is not using GDB.

KDS is using GDB, and here it is up to the launch configuration plugin: it could check if there is already a session running.

This actually is the case for the J-Link connection:

pastedImage_0.png

But so far P&E does not support such a thing yet. My hope is that an upcoming release could have this implemented too.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
853 次查看
BlackNight
NXP Employee
NXP Employee

Hi Peter,

The bad news first: the P&E launch configuration in Eclipse does not support that functionality.

In CodeWarrior, this is handled by the custom debugger engine, and CodeWarrior is not using GDB.

KDS is using GDB, and here it is up to the launch configuration plugin: it could check if there is already a session running.

This actually is the case for the J-Link connection:

pastedImage_0.png

But so far P&E does not support such a thing yet. My hope is that an upcoming release could have this implemented too.

I hope this helps,

Erich

0 项奖励
回复
852 次查看
petershih
Contributor III

Thank you very much!

Peter

0 项奖励
回复