KDS - add C++ support to already existing C project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS - add C++ support to already existing C project

ソリューションへジャンプ
2,569件の閲覧回数
Novalis
Contributor III

Hello,

I am working with USB-MSD demo on FRDM-K64F and I would like to add some C++ code I did to the project. How can I add C++ support to this project? I don't see "Cross ARM C++ compiler" and "Cross ARM C++ linker" in Tool Settings list (just C compiler + linker) under C/C++ build -> Settings -> Tool Settings   just like in new project created by wizzard.

 

I am looking for something easier than creating new project with wizzard and copying all include paths and settings   But if there won't be any other way, I will have to do that.

 

Thanks,

Martin

ラベル(1)
0 件の賞賛
返信
1 解決策
1,977件の閲覧回数
Novalis
Contributor III

Hello,

I found out what I wanted -  I just had  to add line

<nature>org.eclipse.cdt.core.ccnature</nature>

into  .project file  into <natures> section  and now I can also see C++ settings

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,977件の閲覧回数
davenadler
Senior Contributor I

For more complete answer, see: https://community.nxp.com/message/843799 

0 件の賞賛
返信
1,977件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Martin,

Please review following to see if it helps.

How to Create a C++ Project Using MQX RTOS for KSDK1.2

Regards,

David 

0 件の賞賛
返信
1,978件の閲覧回数
Novalis
Contributor III

Hello,

I found out what I wanted -  I just had  to add line

<nature>org.eclipse.cdt.core.ccnature</nature>

into  .project file  into <natures> section  and now I can also see C++ settings

0 件の賞賛
返信