KDS+Processor Expert  MKE02Z to MKE06Z CPU migration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS+Processor Expert  MKE02Z to MKE06Z CPU migration

Jump to solution
1,525 Views
gschelotto
Contributor V

Hi,

 

Months ago I've realized a firmware/hardware MKE02Z project using KDS v3.2 and Processor Expert. Now I'd need to migrate the whole project to MKE06Z (with CAN bus interface). From the point of view of the 64-pin compatibility everything goes well but how can I (painlessly) change the CPU component MKE02Z64VLH4 to MKE06Z64VLH4 as shown?

 

173999_173999.pngUntitled.png

 

I've defined lot of PE components such as Timers, I2C, GPIO, and so on...

regards,

gaston

Labels (1)
0 Kudos
Reply
1 Solution
1,434 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
1,435 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
1,434 Views
gschelotto
Contributor V

Erich, this is exactly what I needed!

Thank you very much,

gaston

0 Kudos
Reply