KDS PE, Linker file and m_cfmprotrom

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KDS PE, Linker file and m_cfmprotrom

跳至解决方案
1,299 次查看
ocmonte
Contributor III

Hello Group!

 

I like using the Processor Expert and would like to know if there is a way to tell PE not to include the m_cfmprotrom sections when creating the linker file? Currently, I'm deleting these sections and managing the linker file manually. I have a boot-loader that manages the m_cfmprotrom section already.

 

TIA

 

Monte--

标签 (1)
0 项奖励
回复
1 解答
1,152 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Monte,

It seems that the section of m_cfmprotrom is generate by default , and it can not control through  PE.

While you can do like this : configure the linker file by manually , then uncheck the "Generate linker file" :

pastedImage_0.png

then the linker file will not changed by the PE, and you can configure the linker file according to your peresonal willingness.

Hope it helps

  .

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,

Alice

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,153 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Monte,

It seems that the section of m_cfmprotrom is generate by default , and it can not control through  PE.

While you can do like this : configure the linker file by manually , then uncheck the "Generate linker file" :

pastedImage_0.png

then the linker file will not changed by the PE, and you can configure the linker file according to your peresonal willingness.

Hope it helps

  .

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,

Alice

0 项奖励
回复
1,152 次查看
ocmonte
Contributor III

Hi Alice!

Yes, that exactly what I'm doing; managing the linker file manually. I just wanted to know if there was a way to disable that from PE. Looks like there is not so I'll continue to manage the linker files.

Thanks for the help.

Cheers,

Monte--

0 项奖励
回复