KDS Debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS Debug problem

Jump to solution
2,086 Views
jackxu
Contributor III

Hello, i'm taking test on MAPS-KS22F256 in KDS (Windows 7), using usb connect with computer and board. when debug j-link, there is a fault point to  connect method via IP

你好,我在调试MAPS-KS22F256时,通过USB与电脑连接,Windows系统下,KDS环境下,Debug时遇到报错,提示通过IP进行连接,但系统通过USB实现(J-Link)

154164_154164.png1.png

154165_154165.png2.png

154181_154181.jpg3.jpg

Labels (1)
0 Kudos
Reply
1 Solution
1,919 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

Please first update the debug interface on bootloader mode :

pastedImage_0.png

If still can not connect , please show your steps .

Hope it helps!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,919 Views
jackxu
Contributor III

Hi Alice,

After following your instruction, can be connected now!

Thanks

Jack

0 Kudos
Reply
1,920 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

Please first update the debug interface on bootloader mode :

pastedImage_0.png

If still can not connect , please show your steps .

Hope it helps!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply