KDS Debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,071件の閲覧回数
jackxu
Contributor III

Hello, i'm taking test on MAPS-KS22F256 in KDS (Windows 7), using usb connect with computer and board. when debug j-link, there is a fault point to  connect method via IP

你好,我在调试MAPS-KS22F256时,通过USB与电脑连接,Windows系统下,KDS环境下,Debug时遇到报错,提示通过IP进行连接,但系统通过USB实现(J-Link)

154164_154164.png1.png

154165_154165.png2.png

154181_154181.jpg3.jpg

ラベル(1)
0 件の賞賛
返信
1 解決策
1,904件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

Please first update the debug interface on bootloader mode :

pastedImage_0.png

If still can not connect , please show your steps .

Hope it helps!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,904件の閲覧回数
jackxu
Contributor III

Hi Alice,

After following your instruction, can be connected now!

Thanks

Jack

0 件の賞賛
返信
1,905件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

Please first update the debug interface on bootloader mode :

pastedImage_0.png

If still can not connect , please show your steps .

Hope it helps!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信