KDS 3.2.0 printing size problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS 3.2.0 printing size problem

1,803 次查看
brunoaguiam
Contributor I

Hi,

Today, I have done a restore defaults in C/C++ Build\Settings in my project for mistake.

After configure some old settings, the printing size and create flash Image didn't work even if selected.

I can't understand what is the problem..Can someone help me.

Best Regards,

0 项奖励
回复
3 回复数

1,733 次查看
brunoaguiam
Contributor I

Hi Erich,

Thank you for your help.

I detect a diference beteween the old makefile and the current.

It looks like the following line is missing: secondary-outputs: $(SECONDARY_FLASH) $(SECONDARY_SIZE).

But i can't set this option on make file.

0 项奖励
回复

1,733 次查看
BlackNight
NXP Employee
NXP Employee

Hi Bruno,

are you able to share your project?

Erich

0 项奖励
回复

1,733 次查看
BlackNight
NXP Employee
NXP Employee

Are you using custom build settings? If yes, then this could be the solution for you: Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse 

Otherwise please share more information (e.g. the console output text you get).

I hope this helps,

Erich

0 项奖励
回复