KDS 3.2.0 - Stepping through Code without Debuger Interface.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 3.2.0 - Stepping through Code without Debuger Interface.

1,346 Views
briancavanagh
Contributor III

Hi, I have been experiencing issues with "No source available for "0x....".   Reading the online comments about this I don't have a way to fix this.  So, this is my question.

Can I step through my C-Code without using the debuger connected to my circuit board?  I'm using the MK22FN256VLH12 uC.  (FYI: If you need to know I'm using the PE Micro Multilink Universal development interface when debuging).

Thanks,

Brian

Tags (2)
0 Kudos
Reply
1 Reply

1,215 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Brain,

KDS doesn't integrated off-line debug simulator. Thus we can't step over code without connecting a board.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply