KDS 3.0 debugger for FRDMK64F stopeed working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0 debugger for FRDMK64F stopeed working

1,779件の閲覧回数
tzahimanistersk
Contributor I

Hi

I've been using KDS 3.0 and KSDK 1.2.0 for FRDM-K64F for a while '

but now I get the folowing error when excecuting "hello wirkd" example.

I get the following error:

56824_56824.pngpastedImage_0.png

 

Please help

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,664件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Or it could be that the gdb client executable you are using cannot be found (does not exist)?

Check as well what is specified in your launch configs.

More on that topic: GDB Client and Server: Unlocking GDB | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信

1,664件の閲覧回数
tzahimanistersk
Contributor I

I've unblocked the GDP according to your advice and it worked!

10X

0 件の賞賛
返信

1,664件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Tzahi Manistersky,

The error message comes from the GDB, it looks that GDB cannot connect to openocd gdb server.

Please, check if after terminate the openocd is still there. If yes, please, try to kill it.

Best Regards,

Iva

0 件の賞賛
返信