KDS 3.0 debugger for FRDMK64F stopeed working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS 3.0 debugger for FRDMK64F stopeed working

1,756 次查看
tzahimanistersk
Contributor I

Hi

I've been using KDS 3.0 and KSDK 1.2.0 for FRDM-K64F for a while '

but now I get the folowing error when excecuting "hello wirkd" example.

I get the following error:

56824_56824.pngpastedImage_0.png

 

Please help

标签 (1)
0 项奖励
回复
3 回复数

1,641 次查看
BlackNight
NXP Employee
NXP Employee

Or it could be that the gdb client executable you are using cannot be found (does not exist)?

Check as well what is specified in your launch configs.

More on that topic: GDB Client and Server: Unlocking GDB | MCU on Eclipse

I hope this helps,

Erich

0 项奖励
回复

1,641 次查看
tzahimanistersk
Contributor I

I've unblocked the GDP according to your advice and it worked!

10X

0 项奖励
回复

1,641 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Tzahi Manistersky,

The error message comes from the GDB, it looks that GDB cannot connect to openocd gdb server.

Please, check if after terminate the openocd is still there. If yes, please, try to kill it.

Best Regards,

Iva

0 项奖励
回复