KDS 3.0.0 not saving .cproject

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0.0 not saving .cproject

1,205件の閲覧回数
glenl
Contributor I

I'm using KDS 3.0.0 with the IAR compiler and have the C-Spy add-in for that. In KDS 2.0, and all previous Eclipse set-up with the IAR tools, changes to its "settings" would have Eclipse save them into the .cproject file. This is not happening with the upgrade to KDS 3.0.0 but worked fine in KDS 2. I've tried "tricking" it to save the .cproject by changing other features in the CDT set-up but it's just not working. Thought to ask if there's a patch or option before I go back to KDS 2.0.

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,085件の閲覧回数
glenl
Contributor I

I'll follow up to say I can't figure this out. I've got two computers and each with KDS 2 and KDS 3 installed. I realized that KDS 2 on one box was saving the .cproject correctly. I carefully analyzed the installed add-ons and version and set the second box version of KDS 2 to be the same. Nope. I have to do all .cproject work on one box and then bounce it through the version control system to make it work. Jave problem? Odd Windows update? Whatever. Can't get it to work.

0 件の賞賛
返信