KDS 2.0 debugger disconnects on entry into LLS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 2.0 debugger disconnects on entry into LLS

2,064 Views
eyaldoron
Contributor II

KDS 2.0 debugger disconnects on entry into LLS (KL15 processor). I'm using the ARM launchpad GNU tools. Is there a way to reconnect automatically, such as was the case for Codewarrior? Otherwise debugging LLS projects is very tricky.

Labels (1)
0 Kudos
Reply
3 Replies

1,967 Views
DavidS
NXP Employee
NXP Employee

Hi Eyal,

In general the KDS does not allow debugger connections when entering low power modes.

If an application is running, there is process for connecting to it but again not when in the low power mode.

Attaching to a Running Target with Segger J-Link, GDB and Eclipse | MCU on Eclipse

Regards,

David

0 Kudos
Reply

1,967 Views
eyaldoron
Contributor II
0 Kudos
Reply

1,967 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Eyal Doron,

I think there was an error while posting your reply and it is empty, could you please try again?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply